The Path to Optimized Site Architecture 400V HVDC Power Solution
Today’s data center and communication facilities are growing faster than ever before. To combat increasing costs at information and communications technology (ICT) sites, data center architects must optimize their power delivery support system without impacting reliability. New and evolving power generation techniques that don’t disrupt data center operations may be the answer.
NetSure ™ HVT 400V HVDC power is designed to ensure the highest levels of system efficiency and reliability. This technology combines the proven benefits of 48V DC power – modularity, scalability, and ease of integration – with the cable and installation cost savings of higher voltage distribution. Based on a flexible architecture, the NetSure HVT power solution can be implemented at a wide variety of different telecom and data center sites.
One of the world’s largest communications services companies that operates in more than 180 countries is densifying its networks for better capacity. Yet, this telco must build its smart network in a way that achieves the lowest throughput cost and the highest availability of service while also being sustainable.
5G is the fifth generation of the cellular telecommunications network, delivering increased bandwidth and faster speeds that enable everything from high-definition video to ultra-low-latency gaming and advanced telemedicine, with the promise for even more advanced applications as the technology matures and expands around the globe.
As we stand on the precipice of a mammoth 5G network transformation, telecom operators, data providers and enterprises are facing new challenges in all areas of the network.